|
Join Keysight principal program manager Rick
Eads, member of the PCI-SIG® board of directors, as he discusses the latest
PCIe® 6.0 developments and what you need to consider when evaluating your
PCIe 6.0 designs. • What are the differences between PCIe® 5.0 and 6.0? • Which industries and applications are driving these changes? • Why is there such a big push to PCIe 6.0 when PCIe 5.0 products are just being released? • How does receiver testing for PCIe 6.0 compare to 5.0? • What additional specifications related to PCIe 6.0 should you be on the lookout for? • When will official compliance testing begin for PCIe 6.0 devices? Register now to learn the latest on PCI Express 6.0 from one of the experts helping to develop the standard. PCI-SIG®, PCIe® and PCI Express® are US registered trademarks and/or service marks of PCI-SIG. |