Desktop banner Mobile banner

EDA Connect 2025 - Massy

March 26, 2025

Whether you are working on radio-frequency integrated circuits (RFIC), monolithic microwave integrated circuits (MMIC), laminate, wafer-level packaging, antennas, or printed circuit boards (PCBs) the integration is becoming denser. This requires circuit simulation to be combined with 3D electromagnetic (EM) simulation to account for inevitable parasitic and coupling effects. Also, validating the system aspects is mandatory to expedite the development cycle.  

In this in-person seminar we will address how Keysight’s EDA software helps to address these challenges. We organize this in cooperation with Altium and Modelithics. The topics include: 

  • Enabling heterogeneous integrated design. 
  • Next generation electromagnetic simulation. 
  • Accelerating the engineering lifecycle with AI/ML. 
  • Simulating with 3D EM and scalable circuit models of SMD Parts. 
  • And more… 

Check out the detailed agenda and register now to save your spot. 

Time

Session

9:00

Reception / Registration                  

9:30

Welcome

9:45

- Enabling Heterogeneous Integrated Design with ADS 
Next Generation EM simulation with ADS RFPro 2025 
Re-imagining RF Design Using ADS Python APIs and AI/ML 
- Transforming Chaos Into Clarity With Keysight Design Data and IP Management 

12:30

Lunch

13:30

- Performance analysis of complex circuit designs through RF line-up simulation 
- Analyzing your PCB layout in Altium Designer (presented by Altium)
- RF Board simulation with 3D EM and scalable circuit models of SMD Parts (presented by Modelithics) 

16:15

Wrap-up


During this seminar we will address some of the latest developments in our Keysight’s EDA software, that help you to make you more efficient when doing your high frequency design. 

Check below the topics we will cover and register. Hope to meet you soon! 

 

Enabling Heterogeneous Integrated Design with ADS 

The demand for higher functionality, smaller sizes, and higher frequency bands in RF and microwave design is driving the need for complex module integration. This paper discusses the challenges and solutions in designing high-frequency applications such as 5G and 6G, automotive radars, and wireless networking.  Keysight's Advanced Design System (ADS) introduces new features in RFPro 3DEM simulation and Smart Mount assembly to address these challenges. These tools enhance simulation accuracy and simplify the integration of different technologies, enabling fast and accurate EM analysis.  The paper highlights how Heterogeneous Integration, combined with these advancements, offers an efficient approach to meeting the stringent requirements of size, weight, power, and cost.  The integration of circuit and 3D EM simulation in ADS facilitates first-pass design success, making it an ideal platform for next-generation heterogeneous integrated module design. 

Next Generation EM simulation with ADS RFPro 2025 

As RF and microwave designs continue to increase in complexity, engineers require tools that streamline workflows and enhance simulation accuracy. RFPro 2025 introduces significant advancements in ADS, enabling more efficient design exploration and validation. This presentation highlights key updates to the Generation 2 Momentum and FEM solvers, including new calibration types that extend accuracy at high frequencies, substrate sweep capabilities for rapid material trade-offs, and the ability to reuse simulation results to save time. Additionally, features such as the modal port solver, enhanced visualization of mesh and fields for MDO simulations, FEM interior meshing, and near and far field computations empower designers to better understand and optimize their designs. Explore how these new capabilities simplify the design process, reduce iteration cycles, and improve confidence in achieving performance targets. 

Re-imagining RF Design Using ADS Python APIs and AI/ML 

As we strive for greater engineering productivity, faster time to market, and optimized decision making from a sea of data – Artificial Intelligence (AI) and Machine Learning (ML) provide exciting new tools to accelerate the engineering lifecycle.  This paper explores how Python APIs in Keysight EDA can transform your workflows, for efficient measurements, design, enterprise, and AI applications, including Machine Learning.  Learn from Keysight customers and industry researchers as they share their successes in application vignettes that will inspire new possibilities for your RF design workflows. 

Transforming Chaos Into Clarity With Keysight Design Data and IP Management 

Ready to revolutionize your design workflow? Discover how a unified data and IP management system can transform the way you work. Imagine having all your design data at your fingertips, perfectly organized and easily accessible, empowering you to create innovative designs with ease. From initial requirements to final tapeout, Keysight's Engineering Lifecycle Management (ELM) acts as your single source of truth, streamlining the entire design process and boosting knowledge sharing. 

Performance analysis of complex circuit designs through RF line-up simulation 

As circuits become more complex, with more requirements to meet under a wider set of conditions, validating the circuit quickly and repeatedly has become a core part of the design process.  Learn more how adding RF line-up simulation to the circuit design workflow can speed up design decisions and time to market. 

ALTIUM's Electronics Lifecycle Management for more innovation and shorter development cycles (presented by Altium) 

Managing data and coordinating business processes across the entire product lifecycle and supply chain are seen as challenges to be addressed. Altium's truly unified approach makes it easy to connect and collaborate with all stakeholders right at the time. Enabling connection to further business tools helps enterprises meet regulatory requirements and maintain high reliability. In addition, Keysight and Altium jointly developed a seamlessly integrated approach to enable every developer with strong Power and Signal Analyzer capabilities to streamlining the path from design to production. This helps you to optimize your development process by making faster and more intelligent decisions with having direct access to analysis capabilities and results. This integrated approach supports concurrent engineering, reducing development cycles and costs while driving 

RF Board simulation with 3D EM and scalable circuit models of SMD Parts (presented by Modelithics) 

The Modelithics COMPLETE+3D Library for Keysight ADS and RFPro incorporates the EM accuracy of 3D components such as SMD inductors and capacitors. Together with RFPro's automatic EM parameterization of substrate etching, dielectric thickness and material properties, RF designers can now efficiently predict the performance impact of manufacturing tolerances and actual purchasable parts with the highest accuracy possible. 

Unlike traditional 3DEM models, the 3D library parts for Keysight ADS also has switchable circuit views for circuit simulation. This enables speedy initial design and optimization with circuit simulators, followed by accurate 3DEM simulation to finalize the design for hardware fabrication. 

 

Co-Sponsor

EDA Connect 2025 - Massy